OPCUA Collector Features

Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.

Summary of OPCUA Collector Features

The following table outlines the features of the OPCUA Collector.

Feature Capability
Browse Source For Tags Yes (on OPCUA Servers that support browsing)
Browse Source For Tag Attributes Yes
Polled Collection Yes
Minimum PollInterval 100 ms
Unsolicited Collection Yes.

If you are using an OPCUA Collector with unsolicited data collection and have collector compression disabled, all new values should produce an exception. When the OPCUA Collector is doing unsolicited collection, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.

Timestamp Resolution 1ms
Accept Device Timestamps Yes
Floating Point Data Yes
Integer data Yes
String data Yes
Binary data Yes
Python Expression Tags Yes
Note: You must set Time Assigned by field to Source if you have unsolicited tags getting data from an OPCUA Collector.

Tag Attributes Available In Browse (OPCUA Data Collectors)

The following table outlines the tag attributes available when browsing.

Attribute Capability
Tagname Yes
Source Address Yes
Polled Collection Yes. See Selecting Data Types
Hi Engineering Units Yes, varies by OPCUA Server Vendor.
Lo Engineering Units Yes, varies by OPCUA Server Vendor.
Hi scale Yes
Lo scale Yes
Is array tag No
Integer data Yes
Note: While some of these attributes are queried on a browse, they are not shown in the browse interface. These attributes are used when adding a tag, but you will not be able to see whether or not all attributes come from the server.

Recommended Data Types

The following table lists the data types recommended for use with Historian.

OPCUA Data Type Recommended Data Type in Historian
I1 - 16 bit signed integer Single integer
I4 - 32 bit signed integer Double integer
R4- 32 bit float Single float
R8- 64 bit double float Double float
UI2- 16 bit unsigned single integer Unsigned single integer
UI4- 32 bit unsigned double integer Unsigned double integer
UI8- 64 bit unsigned quad integer Unsigned quad integer
I8- 64 bit quad integer QuadInteger
BSTR Variable string
BOOL Boolean
I1- 8 bit single integer Byte
Note: The OPCUA Collector requests data from the OPCUA server in the native data type. Then the OPCUA collector converts the received value to a Historian Data Type before sending it to the Data Archiver.