Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / WriteLine Method



In This Topic
    WriteLine Method
    In This Topic
    Writes the supplied value to System.Diagnostics.Trace and to all registered listeners such as file and/or console.
    Overload List
    OverloadDescription
    Writes the supplied value to System.Diagnostics.Trace and to all registered listeners such as file and/or console.  
    Write the supplied subject and value to System.Diagnostics.Trace and to all registered listeners such as file and/or console.  
    Write a message value to System.Diagnostics.Trace depending on supplied trace level.  
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also