Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceWarning Property



In This Topic
    TraceWarning Property
    In This Topic
    Gets whether tracing of warning messages to file is configured, level set to Warning, Info or Verbose.
    Syntax
    'Declaration
     
    Public Shared ReadOnly Property TraceWarning As Boolean
    'Usage
     
    Dim value As Boolean
     
    value = Tracer.TraceWarning
    public static bool TraceWarning {get;}
    public:
    static property bool TraceWarning {
       bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also