Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceOff Property



In This Topic
    TraceOff Property
    In This Topic
    Gets whether tracing to file is currently disabled, level set to Off.
    Syntax
    'Declaration
     
    Public Shared ReadOnly Property TraceOff As Boolean
    'Usage
     
    Dim value As Boolean
     
    value = Tracer.TraceOff
    public static bool TraceOff {get;}
    public:
    static property bool TraceOff {
       bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also