Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceError Property



In This Topic
    TraceError Property
    In This Topic
    Gets whether tracing of error messages to file is configured, level set to Error, Warning, Info or Verbose.
    Syntax
    'Declaration
     
    Public Shared ReadOnly Property TraceError As Boolean
    'Usage
     
    Dim value As Boolean
     
    value = Tracer.TraceError
    public static bool TraceError {get;}
    public:
    static property bool TraceError {
       bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also