Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnFaulted Method
Event source.
Event data.



In This Topic
    OnFaulted Method
    In This Topic
    Invoked when the connection object first enters the faulted states.
    Syntax
    'Declaration
     
    Protected Sub OnFaulted( _
       ByVal sender As Object, _
       ByVal e As EventArgs _
    ) 
    'Usage
     
    Dim instance As ServerConnection
    Dim sender As Object
    Dim e As EventArgs
     
    instance.OnFaulted(sender, e)
    protected void OnFaulted( 
       object sender,
       EventArgs e
    )
    protected:
    void OnFaulted( 
       Object^ sender,
       EventArgs^ e
    ) 

    Parameters

    sender
    Event source.
    e
    Event data.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also