Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnClosed Method
Event source.
Event data.



In This Topic
    OnClosed Method
    In This Topic
    Invoked when the connection object completes transition from the closing to closed states.
    Syntax
    'Declaration
     
    Protected Sub OnClosed( _
       ByVal sender As Object, _
       ByVal e As EventArgs _
    ) 
    'Usage
     
    Dim instance As ServerConnection
    Dim sender As Object
    Dim e As EventArgs
     
    instance.OnClosed(sender, e)
    protected void OnClosed( 
       object sender,
       EventArgs e
    )
    protected:
    void OnClosed( 
       Object^ sender,
       EventArgs^ e
    ) 

    Parameters

    sender
    Event source.
    e
    Event data.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also