Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / IsConnected Method



In This Topic
    IsConnected Method
    In This Topic
    Whether currently connected to a Historian server.
    Syntax
    'Declaration
     
    Public Function IsConnected() As Boolean
    'Usage
     
    Dim instance As ServerConnection
    Dim value As Boolean
     
    value = instance.IsConnected()
    public bool IsConnected()
    public:
    bool IsConnected(); 

    Return Value

    True if connected.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also