Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / Disconnect Method



In This Topic
    Disconnect Method
    In This Topic
    Disconnect from a Historian server.
    Syntax
    'Declaration
     
    Public Sub Disconnect() 
    'Usage
     
    Dim instance As ServerConnection
     
    instance.Disconnect()
    public void Disconnect()
    public:
    void Disconnect(); 
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also