Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / DataChangedEvent Event



In This Topic
    DataChangedEvent Event (ServerConnection)
    In This Topic
    Occurs in response to data subscriptions when the latest tag value has been updated.
    Syntax
    'Declaration
     
    Public Event DataChangedEvent As DataChangedHandler
    'Usage
     
    Dim instance As ServerConnection
    Dim handler As DataChangedHandler
     
    AddHandler instance.DataChangedEvent, handler
    public event DataChangedHandler DataChangedEvent
    public:
    event DataChangedHandler^ DataChangedEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also