Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / CollectorHierarchicalBrowseResponseEvent Event



In This Topic
    CollectorHierarchicalBrowseResponseEvent Event (ServerConnection)
    In This Topic
    Occurs when a collector responds with hierarchical tag browse information.
    Syntax
    'Declaration
     
    Public Event CollectorHierarchicalBrowseResponseEvent As CollectorHierarchicalBrowseResponseHandler
    'Usage
     
    Dim instance As ServerConnection
    Dim handler As CollectorHierarchicalBrowseResponseHandler
     
    AddHandler instance.CollectorHierarchicalBrowseResponseEvent, handler
    public event CollectorHierarchicalBrowseResponseHandler CollectorHierarchicalBrowseResponseEvent
    public:
    event CollectorHierarchicalBrowseResponseHandler^ CollectorHierarchicalBrowseResponseEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also