Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IPublish Interface / PublishSetDestinationServerEvent Event



In This Topic
    PublishSetDestinationServerEvent Event (IPublish)
    In This Topic
    Occurs when a collector responds to setting a destination server name.
    Syntax
    'Declaration
     
    Event PublishSetDestinationServerEvent As PublishSetDestinationServerHandler
    'Usage
     
    Dim instance As IPublish
    Dim handler As PublishSetDestinationServerHandler
     
    AddHandler instance.PublishSetDestinationServerEvent, handler
    event PublishSetDestinationServerHandler PublishSetDestinationServerEvent
    event PublishSetDestinationServerHandler^ PublishSetDestinationServerEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also