Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / EnumeratedSetChangedEvent Event



In This Topic
    EnumeratedSetChangedEvent Event (IEnumeratedSets)
    In This Topic
    Occurs in response to enumerated set subscriptions when a set has been added, deleted or modified.
    Syntax
    'Declaration
     
    Event EnumeratedSetChangedEvent As EnumeratedSetChangedHandler
    'Usage
     
    Dim instance As IEnumeratedSets
    Dim handler As EnumeratedSetChangedHandler
     
    AddHandler instance.EnumeratedSetChangedEvent, handler
    event EnumeratedSetChangedHandler EnumeratedSetChangedEvent
    event EnumeratedSetChangedHandler^ EnumeratedSetChangedEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also