Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IArchives Interface / DropSubscriptions Method



In This Topic
    DropSubscriptions Method (IArchives)
    In This Topic
    Drop all the archive subscriptions.
    Syntax
    'Declaration
     
    Sub DropSubscriptions() 
    'Usage
     
    Dim instance As IArchives
     
    instance.DropSubscriptions()
    void DropSubscriptions()
    void DropSubscriptions(); 
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also