Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IArchives Interface / BackupConfig Method
Backup file name to create.



In This Topic
    BackupConfig Method
    In This Topic
    Create a backup of the configuration.
    Syntax
    'Declaration
     
    Sub BackupConfig( _
       ByVal backupFilename As String _
    ) 
    'Usage
     
    Dim instance As IArchives
    Dim backupFilename As String
     
    instance.BackupConfig(backupFilename)
    void BackupConfig( 
       string backupFilename
    )
    void BackupConfig( 
       String^ backupFilename
    ) 

    Parameters

    backupFilename
    Backup file name to create.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also