Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IArchives Interface / ArchiveChangedEvent Event



In This Topic
    ArchiveChangedEvent Event (IArchives)
    In This Topic
    Occurs in response to archive subscriptions when an archive has been added, deleted or modified.
    Syntax
    'Declaration
     
    Event ArchiveChangedEvent As ArchiveChangedHandler
    'Usage
     
    Dim instance As IArchives
    Dim handler As ArchiveChangedHandler
     
    AddHandler instance.ArchiveChangedEvent, handler
    event ArchiveChangedHandler ArchiveChangedEvent
    event ArchiveChangedHandler^ ArchiveChangedEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also