Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianFault Class / ToString Method



In This Topic
    ToString Method (HistorianFault)
    In This Topic
    Converts the value of this instance to a System.String.
    Syntax
    'Declaration
     
    Public Overrides Function ToString() As String
    'Usage
     
    Dim instance As HistorianFault
    Dim value As String
     
    value = instance.ToString()
    public override string ToString()
    public:
    String^ ToString(); override 

    Return Value

    A string representation of this instance.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also