Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / ServerVersion Field



In This Topic
    ServerVersion Field
    In This Topic
    The version of a Historian server.
    Syntax
    'Declaration
     
    <DataMemberAttribute()>
    Public ServerVersion As String
    'Usage
     
    Dim instance As HistorianConfiguration
    Dim value As String
     
    value = instance.ServerVersion
     
    instance.ServerVersion = value
    [DataMember()]
    public string ServerVersion
    [DataMember()]
    public:
    String^ ServerVersion
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also