Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / EnumeratedSetLastModifiedUser Field



In This Topic
    EnumeratedSetLastModifiedUser Field
    In This Topic
    The name of the last user to modify the enumerated set configuration in a Historian server.
    Syntax
    'Declaration
     
    <DataMemberAttribute()>
    Public EnumeratedSetLastModifiedUser As String
    'Usage
     
    Dim instance As HistorianConfiguration
    Dim value As String
     
    value = instance.EnumeratedSetLastModifiedUser
     
    instance.EnumeratedSetLastModifiedUser = value
    [DataMember()]
    public string EnumeratedSetLastModifiedUser
    [DataMember()]
    public:
    String^ EnumeratedSetLastModifiedUser
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also