Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / ActualDataStores Field



In This Topic
    ActualDataStores Field
    In This Topic
    The current number of data stores configured.
    Syntax
    'Declaration
     
    <DataMemberAttribute()>
    Public ActualDataStores As Long
    'Usage
     
    Dim instance As HistorianConfiguration
    Dim value As Long
     
    value = instance.ActualDataStores
     
    instance.ActualDataStores = value
    [DataMember()]
    public long ActualDataStores
    [DataMember()]
    public:
    int64 ActualDataStores
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also