Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataSubscriptionInfo Class / MinimumElapsedMilliSeconds Property



In This Topic
    MinimumElapsedMilliSeconds Property
    In This Topic
    The minimum number of milliseconds between successive updates. Used to throttle high frequency tags.
    Syntax
    'Declaration
     
    <DataMemberAttribute()>
    Public Property MinimumElapsedMilliSeconds As Integer
    'Usage
     
    Dim instance As DataSubscriptionInfo
    Dim value As Integer
     
    instance.MinimumElapsedMilliSeconds = value
     
    value = instance.MinimumElapsedMilliSeconds
    [DataMember()]
    public int MinimumElapsedMilliSeconds {get; set;}
    [DataMember()]
    public:
    property int MinimumElapsedMilliSeconds {
       int get();
       void set (    int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also