Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataSet Class / AddRange Method
A source collection.



In This Topic
    AddRange Method (DataSet)
    In This Topic
    Adds all elements from the given collection to the end this instance.
    Syntax
    'Declaration
     
    Public Sub AddRange( _
       ByVal dataset As DataSet _
    ) 
    'Usage
     
    Dim instance As DataSet
    Dim dataset As DataSet
     
    instance.AddRange(dataset)
    public void AddRange( 
       DataSet dataset
    )
    public:
    void AddRange( 
       DataSet^ dataset
    ) 

    Parameters

    dataset
    A source collection.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also