Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQueryParams Class / Criteria Property



In This Topic
    Criteria Property (DataQueryParams)
    In This Topic
    A set of criteria defining the data query.
    Syntax
    'Declaration
     
    Public Property Criteria As DataCriteria
    'Usage
     
    Dim instance As DataQueryParams
    Dim value As DataCriteria
     
    instance.Criteria = value
     
    value = instance.Criteria
    public DataCriteria Criteria {get; set;}
    public:
    property DataCriteria^ Criteria {
       DataCriteria^ get();
       void set (    DataCriteria^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also