Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataCriteria Class


In This Topic
    DataCriteria Class Fields
    In This Topic

    For a list of all members of this type, see DataCriteria members.

    Public Fields
     NameDescription
    Public Field Establish whether to resolve a query in backward time order (true) or forward time order (false).  
    Public FieldEstablish a calculation mode for a query. See DataCriteria.CalculationModeType.  
    Public Field Establish an end time for a query.  
    Public FieldEstablish a filter comparison mode for a query. See DataCriteria.FilterComparisonModeType.  
    Public FieldEstablish a constant value to filter a query. This value is compared using FilterComparisonMode.  
    Public FieldProvide a complete filter Expression to query on. This is independent of the FilterTag. When the Filterexpression is set a FilterComparisonMode or FilterComparisonValue should not be provided. e.g. (Testag1 > 5000)  
    Public FieldEstablish a filter mode for a query. See DataCriteria.FilterModeType.  
    Public FieldEstablish a tag name to filter a query. Filtered tag queries evaluate the value of the filter tag against a constant comparison value and only retain time intervals where this comparison evaluates true. Filtered tag queries are further modified by DataCriteria.FilterModeType and DataCriteria.FilterComparisonModeType.  
    Public Field  
    Public Field Establish a number of milliseconds between data samples for a query.  
    Public Field  
    Public Field Establish a number of data samples to retrieve for a query.  
    Public Field Establish the QueryModifiers to a query.  
    Public FieldEstablish a sampling mode for a query. See DataCriteria.SamplingModeType.  
    Public Field Establish a start time for a query.  
    Public Field Establish a value to for the calculation mode Statevalue or StateCount.  
    Public Field Establish a set of tag names for a query.  
    Top
    See Also