Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ArchiveQueryParams Class / Namemask Property



In This Topic
    Namemask Property (ArchiveQueryParams)
    In This Topic
    Constrains the list of archives returned based on archive name. The standard wildcard characters ? (matches 1 character) and * (matches any number of characters) may be used.
    Syntax
    'Declaration
     
    Public Property Namemask As String
    'Usage
     
    Dim instance As ArchiveQueryParams
    Dim value As String
     
    instance.Namemask = value
     
    value = instance.Namemask
    public string Namemask {get; set;}
    public:
    property String^ Namemask {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also