Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmCriteria Class / EventCategoryCriteria Property



In This Topic
    EventCategoryCriteria Property
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("EventCategoryCriteria")>
    Public Property EventCategoryCriteria As StringCriteria
    'Usage
     
    Dim instance As AlarmCriteria
    Dim value As StringCriteria
     
    instance.EventCategoryCriteria = value
     
    value = instance.EventCategoryCriteria
    [DataMember("EventCategoryCriteria")]
    public StringCriteria EventCategoryCriteria {get; set;}
    [DataMember("EventCategoryCriteria")]
    public:
    property StringCriteria^ EventCategoryCriteria {
       StringCriteria^ get();
       void set (    StringCriteria^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also