Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmAttribute Class / ValueCriteria Property



In This Topic
    ValueCriteria Property
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("ValueCriteria")>
    Public Property ValueCriteria As Object
    'Usage
     
    Dim instance As AlarmAttribute
    Dim value As Object
     
    instance.ValueCriteria = value
     
    value = instance.ValueCriteria
    [DataMember("ValueCriteria")]
    public object ValueCriteria {get; set;}
    [DataMember("ValueCriteria")]
    public:
    property Object^ ValueCriteria {
       Object^ get();
       void set (    Object^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also