TYPE NAME |
Enter a name for the user-defined data type
(UDT). |
DESCRIPTION |
Enter a description for the UDT. |
ADMINISTER GROUP |
Specify the Windows Security Group that you want to
assign to the UDT. |
DATA QUALITY |
Select one of the following options:
- Store Individual Quality:
Select this option to store field-level quality.
Storing individual qualities consumes more disk
space.
- Store Master Field Quality:
Select this option if you want to assign the same
quality as the master field to all the other fields
in the UDT. If you select this option, the data
sample will have a single quality similar to how an
array tag works.
|
MASTER |
Select the radio button corresponding to the field that
you want to set as master. When you do so, the data type of
this field is used for all the remaining fields in the UDT
as well. Only one field can be the master in a UDT. The
MASTER column appears only if you
select Store Master Field Quality
under DATA QUALITY. |
NAME |
Enter a name for the field. |
DESCRIPTION (under
FIELD) |
Enter a description for the field. |
DATA TYPE |
Select the data type for the field. If you select
Store Master Field under
DATA QUALITY, and if you set this
field as master, the data type of this field will be applied
to the remaining fields in the UDT as well. |