By default, the duration used for items in a display is one hour up to the current time.
You can choose of the following durations:
One hour
Eight hours
One day
One week
One month
In addition, you can set the start and end dates and
timezone.
Procedure
Select Tags, and then select one of the
following durations:
1h (one hour)
8h (eight hours)
1d (one day)
1w (one week)
1m (one month)
The items in the display are plotted for the selected
duration.
If you want to change the start and end dates:
Select Time.
Enter values in the
Start and
End fields.
If you want to apply the start and end dates
only for the selected item, select
Apply. If you want to apply
the changes to all the items in the display,
select Apply to All.