You can reconnect to the ODBC server automatically as soon as the server is up and running.
By default, the collector polls for the server connection every 5
seconds. You can change this interval as well. The collector is
stopped until reconnected to the server.
Procedure
Access the following registry key:
HKEY_LOCAL_MACHINE\SOFTWARE\GE
Digital\iHistorian\Services\ODBCCollector.
Create a DWORD named
EnableReconnect.
Enter the decimal value 1.
If you want to change the reconnection interval (from
the default value of 5 seconds):
Create a DWORD named
ReconnectInterval.
Enter a decimal value between 5 and 60. This
value represents the number of seconds for the
collector to wait before trying to reconnect to
the ODBC server.