Resolved Issues

Description Tracking ID
Previously, even if you disabled future data, when you attempted to collect future data, instead of displaying an error message, a success message was displayed although future data was not stored. This issue has been resolved in Historian 2023. DE138535
Previously the Data Archiver crashed when querying for more than one collector. This issue has been resolved in Historian 2023. DE165564
Previously, the option to recalculate was disabled for iHTagAdmin users. This issue has been resolved by changing the security and user permissions. DE167016
Previously, there were issues in the OPC UA HDA collector redundancy. These issues have been resolved. DE168191
Previously, if you updated the collection interval and compression values, tag data was not collected. This issue has been resolved. DE170431
Previously, a login to the Archiver with no user failed (Security message which says that Unknown (\) failed login). This issue has been resolved in Historian 2023. DE154221
Previously, the ifixAEcollector.exe shut down from time-to-time. This issue has been resolved in Historian 2023. DE178154
Previously, when trying to create a chart in the Historian Trend Client while using domain security an "Unkown error" message appeared. This issue has been resolved in Historian 2023. DE184585
Previously, the Excel Add-In threw an error “Compile error in hidden module: frmTagSearch.” This issue has been resolved in Historian 2023. DE184584
When Historian switched to a new archive, calculations stop working. Bad CalcFailed is received on the calculation. DE176969
Previously, memory consumption is high for the Diagnostic Manager. Optimizations were done to minimize memory consumption of this service. DE177422
The Calculation Collector ignores the data quality. These tags have good values in Historian Administrator for 'Last 10 values'. To solve it, we restarted the OPC Kepware collector. DE175743
Previously, memory consumption was high for the UA HAD Server. Optimizations were done to minimize memory consumption of this service. DE185245
Previously, memory consumption was high for Client Manager. Optimizations were done to minimize memory consumption of this service. DE187941
The HDA Collector shut down when adding a new tag. This issue has been resolved in Historian 2023. DE181238
The Filtered Data dialog was not displayed properly in Proficy Historian Excel Add-in. This issue has been resolved in Historian 2023. DE173096
When browsing the tag on the Historian, Swedish characters appears as ?? instead of the real characters. This issue has been resolved in Historian 2023. DE191441
The OLE-DB provider query failed when a non-existing tag was in the first position. This issue has been resolved in Historian 2023. DE183849
Issues with OPC redundancy have been fixed in Historian 2023. DE188552
Previously, a Linked Server - access denied (c000005) with SQL 2016 message may appear. This issue has been resolved in Historian 2023. DE186000
Previously, the Server-Server Collector was not working properly. This issue has been resolved in Historian 2023. DE191561
Historian 2023 includes support for the FMG Query regarding the upcoming DCOM hardening from Microsoft (CVE-2021-26414). DE178873
Previously, the OLE DB problem max value query did not send output to what was the expected result. This issue has been resolved in Historian 2023. DE121596
Previously, the OPC UA Collector could not handle handle Swedish letters. This issue has been resolved in Historian 2023. DE121597
Previously, when a connection from the OPC Server to the PLC was broken, data in Historian still had a quality flag "Good". It's now it’s fixed. DE125668
Previously, we were getting the actor field set to null from ihSql. This issue has been resolved in Historian 2023. DE171154
Previously, ihSql was providing an alarm type= Alarm history - API Error. This issue has been resolved in Historian 2023. DE168388
Previously, the Alarm Backup, Purge, and Restore operation did not return the A&E Database to its previous status. This issue has been resolved in Historian 2023. DE109010
Previously, random duplicate Alarm Comments generated. This issue is now fixed to eliminate duplicate alarm comments. DE120509
Previously, the SQL Server A&E Database result could become corrupt and was not able to get all Alarms & Events information. This issue has been resolved in Historian 2023. DE128453
Previously, the Upgrade AEDB 6.0 - 8.0 - Emergency Stop Requested was not included in the VerifyScriptsLog.log. This issue has been resolved in Historian 2023. DE186522
Previously, index timeouts during install resuled in performance issues. This issue has been resolved in Historian 2023. DE186523
Using Configuration Hub, you cannot define a calculation formula for a tag for a Calculation collector. You can, however, define a calculation formula using Historian Administrator or other Web-based Clients. DE171279
Previously, when a user logged in to Historian Web Admin or Trend Client and did not have permissions, the following message appeared: "Access Denied: Insufficient privileges for the user." The spelling of this error has been corrected in Historian 2023. DE181771
Previously, in the presence of Security groups, the ihTagAdmin users were not able to see tag details in the third panel in Configuration Hub. This has been resolved in Historian 2023. DE189223
Previously, the Historian Web Administrator did not accept negative values for the Engineering Unit Range. This has been resolved in Historian 2023. DE177133
Previously, the Time selection in web Trend Client was not possible. In Historian 2023, trending moved from the Trend Client to Configuration Hub. the new architecture resolves this issue. DE197676
Previously, installation of Operation Hub 2022 was failing. It is now resolved in Historian 2023. DE197675
Previously, after adding an OPC UA Collector in Configuration hub, the Secured Connectivity and User Security options could not be changed. This issue has now has been resolved in Historian 2023. DE177011
Previously, when you added File Collector tags via Configuration Hub (via the Add Manually option), you were unable to associate those tags with the File Collector. This issue has been resolved in Historian 2023. DE179318