Jobs Page
When you add a mirror node, replicate a node, re-synch an archive file, back up an archive file or restore an archive file then a job is initiated with a Job ID, which will be seen on the user interface of the Historian Web Admin console.
To view the jobs, you can select the Active Jobs link in any of the Collector, Client, or Configuration pages. You can view the number of jobs that are currently running on the system from this page and can also search a job based on its Job ID by entering the Job ID and selecting the search button in the search field.
Field | Description |
---|---|
Status | Displays the current status of the job (Succeeded, Failed and In Progress) in different color codes. If you see a Failed job, you can expand it to see the description of the failure. |
Job ID | The unique ID given to a particular job. |
Type | The type of job. |
Description | The description of the job. |
Percentage | The percentage of completion of the job. |
Start Time | The time at which the job started. |
Complete Time | The time at which the job was completed. |