Microsoft Excel
With Excel, you can import a snapshot of Historian data at a single point in time. You can choose Historian as a data source in Excel. You can specify the connection settings manually or using a UDL file.
After you import the data, you can create and edit SQL queries in Excel.
When to Use Excel Instead of the Historian Excel Add-In
Use the Excel Add-In when you want to get data into Microsoft Office 2003, 2007 or 2010 (32-bit/64-bit). Use the Historian OLE DB provider with Excel, instead of the Excel Add-In, when you want to do any of the following:
- Perform advanced filtering, sorting, and joining of data.
- Obtain detailed information from the ihTrend table.
- Run calculations using the SQL aggregate functions.
- Perform advanced summaries.
File Name | Description |
---|---|
ihOLEDB_ LASTHOUR.XLS | One-sheet report that uses auto-refresh to display the last hour of data using relative shortcuts. |
ihTags.odc | Data source file that retrieves the ihTags table from the default server. |
iHistorian.udl | Sample universal data link (.UDL) file that connects to the default Historian server with the currently logged-in user. |
These sample are found in the following folder: Historian\Samples\Excel