Restore the Alarms and Events Data
Install Microsoft SQL. Refer to Software Requirements for a list of supported versions.
Procedure
-
Go to the <Historian installation folder>\Proficy DataBase folder, and open the Proficy.Historian.AandE.Migration.exe file.
The Backup Existing Alarms and Events window appears.
- Select Migrate Alarms and Events Backup.
- In the Backup Folder Path field, provide the absolute path of the file (including the file name) in which you want to restore the data (for example, c:\temp\March2010.bak). You can enter the path of a local file or a remote one, depending on whether the Microsoft SQL server is installed on the local machine or a remote machine.
- In the Database Name field, enter the name of the database that you want to back up. Typically, this value is the same as the Microsoft SQL server you are using.
- Depending on whether you want to use Windows credentials or Microsoft SQL credentials, select either Use Windows Authentication or Use SQL Authentication, respectively.
- In the User Id and Password fields, enter the login credentials. Provide the username of a user who has the permission to connect and back up alarms.
-
Select Test Connection to check if the source database is active and the information is accurate.
The Begin Migrator button is activated.
-
Select Begin Migrator.
The alarms and evens data is restored. The count of the rows that are restored appears.