Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
You can reconnect to the OPC Classic HDA
server automatically as soon as the server is up and running. By default, the collector
polls for the server connection every 5 seconds. You can change this interval as well.
The collector is stopped until reconnected to the server.
Procedure
Access the following registry key: HKEY_LOCAL_MACHINE\SOFTWARE\GE
Digital\iHistorian\Services\OPCHDACollector.
Locate the Key created with the ProgID of the OPC Classic HDA
server.
Create a DWORD named EnableOPCHDAReconnect.
Enter the decimal value 1.
If you want to change the reconnection interval (from the default value of 5
seconds):
Create a DWORD named ReconnectInterval.
Enter a decimal value between 5 and 60. This value represents the
number of seconds for the collector to wait before trying to reconnect
to the OPC server.