Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
In the OPC UA HDA server, the flat address space is
used by default. This type of model is used to browse a small number of tags. If
you want to browse a large number of collectors and tags, enable the hierarchical
address space.
Procedure
Access Registry, and then go to the following key folder: .
For Windows (32-bit): HKEY_LOCAL_MACHINE\SOFTWARE\Intellution,
Inc.\iHis- torian\HDAServer\
For Windows (62-bit): HKEY_LOCAL_
MACHINE\SOFTWARE\Wow6432Node\\Intellution,
Inc.\iHistorian\HDAServer\
Create a DWORD named HierarchicalAddressSpace.
In the Value box, enter
255.
Note: For a flat address space, this value is set to 0.
Select OK, and then close the Registry.
Restart the OPC Classic HDA
server by disconnecting and reconnecting all the
OPC HDA clients.