Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
You can authenticate a user based on one of the following methods:
User credentials: In this method, you will use the credentials of a
Historian user. When you do so, the OPC UA HDA server validates the credentials
by connecting to the Historian server, and then grants access.
Note: The user is
authenticated regardless of whether the Historian server is part of a
stand-alone or a distributed Historian system.
Certificate: In this method, you will provide a trusted certificate and a
private key of the OPC UA HDA server. The server validates that the certificate
is the same as the user certificate stored in the server, and then grants
access.
Tip: You can generate a self-signed certificate and its
keys using the Proficy Historian OPC UA Server
Configuration tool, which is provided with the OPC UA HDA
server.
Anonymous authentication is not supported.
Procedure
Access the OPC UA HDA client.
If you want to authenticate a user using the user credentials, select the
appropriate option in the user authentication window, and then enter the
username and password of the Historian user.
If you want to authenticate a user using a certificate:
Select the appropriate option in the user authentication window.
Provide the certificate and the private key (which are stored in the
.der and .pem formats respectively). If needed, enter a password for the
private key.
Results
The user is authenticated. A list of Historian tags appears
in the OPC UA HDA client. These tags are represented as models in the client,
categorized based on the data type. The OPC UA HDA server collects tag data from Historian, and sends it to the client. You can now use the
client to access a trend chart of the tag data and analyze it.