Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
Historian allows you to specify the maximum disk cache memory that an archiver can use. By default, Historian consumes 25% of system memory. If your computer has extra memory, then you can increase the disk cache. Increasing the disk cache memory optimizes the Historian performance. You should not increase system file caching cache memory if you do not have the necessary system resources.
Procedure
On the Start menu, select Run, type Regedit, and then select OK.
The Registry editor appears.
Open the following key folder.HKEY_LOCAL_MACHINE\SOFTWARE\Intellution, Inc.\iHistorian\Services\DataArchiver\
Create a new DWORD called FileSystemMaxCacheMB
Set the decimal value to a number. The value that you enter represents the maximum disk cache memory that an archiver can use.