Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
In this example, you calculate a value (such as an hourly average of a source tag)
or add two source tags together.
Procedure
Using Historian Administrator, add a tag manually to the destination, as shown in the following
image:
In the Tags section, select
Collection.
In the Collection Type box, select
Polled.
Set the Collection Interval to 1 hour.
Select Calculation.
In the Calculation section, enter the name of the tag,
or use the Insert Function Wizard to browse and select
the tagname. Then, build your calculation formula.
The following figure shows an example of inserting a calculated value
for a tag with the Insert Function Wizard.
Select Insert.
The Tag Maintenance page appears, showing the
formula in the Calculation section.
Select Update to save your changes.
A message appears, asking you if you want to test the
formula.
Select Yes.
The Server-to-Server collector will begin processing the created tag upon the next collector
reload.