ihEnumeratedSets Table
The ihEnumeratedSets table contains information about enumerated sets that are defined in the system. The following table describes the columns of the ihEnumeratedSets table.
Column Name | Data Type | Description |
---|---|---|
SetName | VT_BSTR | The name of the set. |
Description | VT_BSTR | The description of the set. |
NumberofStates | VT_I4 | The number of states a set contains. |
NumberofTagReferences | VT_I4 | The number of tags with which a set is associated. |
SetDataType | VT_BSTR | The data type of the set. |
AdministratorSecurityGroup | VT_BSTR | The security group to which the set belongs. |
LastModifiedUser | VT_BSTR | Indicates which user last modified the set. |
LastModifiedTime | VT_DBTimeStamp | Indicates the last time the set was modified. |
RowCount | VT_I4 | Indicates the maximum number of rows that can be returned. A value of 0 indicates that there is no limit to the number of rows returned. |
ihEnumeratedSets Examples
Sample SQL statements for the ihEnumeratedSets table are outlined in the following examples.
Example 1: Retrieve All Sets By Using Integer States
SELECT * FROM ihEnumeratedSets
WHERE SetDataType=’integer’
Example 2: Retrieve a Set By Name From Sets
SELECT * FROM ihEnumeratedSets
WHERE setname like PLC1