Alarms Object
You can use Historian to store data for alarms and events. From the SDK, you can add and query these alarms and events. This class is slightly different from other SDK classes in that you will mostly be accessing lower level functionality to add and query alarms and events. By following the directions below, you should be able to perform these tasks fairly easily.
Add Historian Type Library to the Project
As previously mentioned, access to methods for alarms and events is lower level. You must add the Historian COM 1.1 Type library to your project. In Visual Basic, in the Project menu, select References, and then add the library. You can now access the lower level alarms and events methods.
Query by Alarms and Events
For instructions on querying alarms and events, see the documentation for the AlarmRecordSet function.
Add Alarms and Events
You can add alarms and events to Historian by using the AlarmInfo object. In general, adding alarms or events is easy; declare a new AlarmInfo object, fill it up with the required details, and then run the Add function on the AlarmInfo object. In practice, you must be aware of the lifecycle of your alarm.
Create a new AlarmInfo Object
To create a new AlarmInfo object, use the CreateObject method as follows:
Dim myAlarmInfo As AlarmInfo
Set myAlarmInfo = CreateObject("Historian_API.AlarmInfo")
Alarm or Event?
Historian distinguishes between alarms and events. Alarms follow a lifecycle as described below, while events are generally one-shot deals. Example events include Set Point Events, Login Events, or other audit trail events. Alarms are generally characterized by a tag going into and out of an abnormal condition. You must identify your AlarmInfo object as an alarm or event by setting the AlarmType field.
Alarm:myAlarmInfo.AlarmType = ihALARM_CONDITION
Event: myAlarmInfo.AlarmType = ihALARM_TRACKING
Alarm Life Cycle
myAlarmInfo.AddMyServer myAlarmInfo.Clear
New AlarmTo instantiate a new alarm, specify the start time in the AlarmInfo object.
myAlarmInfo.StartTime= Now
State Change
myAlarmInfo.SubConditionName= "HIHI"
Wrong:'myAlarmInfo.StartTime= Now
OK:'myAlarmInfo.StartTime=AlarmStartTime
Acknowledge an Alarm
To acknowledge an alarm, set the Acked field in the AlarmInfo to True, and also specify the time of the acknowledgement by populating the AckTime alarm field. In addition, you must populate the starttime field with the start time of the alarm (when it first went into an alarm condition, not the last state change).
myAlarmInfo.Acked= TRUE
myAlarmInfo.AckTime = Now
myAlarmInfo.StartTime = AlarmStartTime
Return to Normal
When your alarm condition has ended, specify the endtime in the AlarmInfo Object. Similar to the state change and acknowledgements, you can optionally specify the start time of the alarm in the starttime alarm field.
myAlarmInfo.EndTime= Now myAlarmInfo.StartTime = AlarmStartTime
Associating Alarms and Events with Tag Data
The easiest way to associate alarms and events with tag data is to specify the TagName in the AlarmInfo. Historian will sort out everything behind the scenes. However, if you are adding alarms before the associated tag actually exist in Historian, this avenue will not work. You must populate the ItemId field with the source address of the future tag, and populate the DataSourceName field with the collector name of the tag. When the tag is added to the system, the alarms will be correctly linked.
myAlarmInfo.Tagname = TheTagName
OrmyAlarmInfo.DataSourceName = MyCollector.Name myAlarmInfo.ItemId = TheSourceAddress
AlarmInfoFields
The following table lists the AlarmInfo fields. The fields that are marked as required must be filled in for every call to add. In addition, populate the correct fields based on the current state in the lifecycle of your alarm (see above).
FieldName | Data Type | Required for Alarms or Events? | Description |
---|---|---|---|
AlarmType | Long | Both | Classifies this AlarmInfo as an alarm or an event. Enter 1 for an event and 4 for an alarm. |
ItemID | String | None | The ItemID of the alarm or event. This contains the source address of the data access tag that the alarm is associated with. This can be NULL if the alarm is not associated with a tag. |
Source | String | Both | This is the unique identifier used for the alarm or event. |
DataSourceName | String | Both | The collector interface name associated with the alarm or event. |
Tagname | String | None | The Historian Tag Name associated with the alarm. |
EventCategory | String | None | The event category of the alarm or event. |
ConditionName | String | Alarms | The condition of the alarm. This does not apply to event data. This, combined with the source, comprises an alarm. |
SubConditionName | String | Alarms | The sub-condition of the alarm. This does not apply to event data. This is the state of the alarm. |
StartTime | Date | None | The start time or time stamp of the alarm or event. |
EndTime | Date | None | The end time of the alarm. This does not apply to event data. |
AckTime | Date | None | The time the alarm was acknowledged. This does not apply to event data. |
Timestamp | Date | Both | The time stamp of the alarm or event. |
Message | String | None | The message attached to the alarm or event. |
Acked | Boolean | None | Stores the acknowledgement status of the alarm. If the alarm is acknowledged, this will be set to TRUE. |
Severity | Long | None | The severity of the alarm or event. This is stored as an integer value with a range of 1-1000. |
Actor | String | The operator who acknowledged the alarm, or caused the tracking event. | |
Quality | Long | Alarms | The quality of the alarm or event. 0 for bad, 3 for good. |
Dim MyServer As iHistorian_SDK.Server
Set MyServer = GetServer
Dim myAlarmInfo As AlarmInfo
Set myAlarmInfo = CreateObject("iHistorian_API.AlarmInfo")
Dim AlarmStartTime As Date
AlarmStartTime = Now
' New Alarm myAlarmInfo.AlarmType = ihALARM_CONDITION
myAlarmInfo.ConditionName = "SampleCondition"
myAlarmInfo.DataSourceName = "SampleDataSource"
myAlarmInfo.Message = "Sample Alarm"
myAlarmInfo.Source = "SampleSource"
myAlarmInfo.StartTime = AlarmStartTime
myAlarmInfo.SubConditionName = "HI"
myAlarmInfo.Timestamp = Now
myAlarmInfo.Quality = 3
myAlarmInfo.Add MyServer
myAlarmInfo.Clear
' State Change myAlarmInfo.AlarmType = ihALARM_CONDITION
myAlarmInfo.ConditionName = "SampleCondition"
myAlarmInfo.DataSourceName = "SampleDataSource"
myAlarmInfo.Message = "Sample Alarm State II"
myAlarmInfo.Source = "SampleSource"
' Not required, but pointing out the start time of the alarm doesn't hurt
myAlarmInfo.StartTime = AlarmStartTime
myAlarmInfo.SubConditionName = "HIHI"
myAlarmInfo.Timestamp = Now
myAlarmInfo.Quality = 3
myAlarmInfo.Add MyServer
myAlarmInfo.Clear
' Ack the HIHI state
myAlarmInfo.Acked = True
myAlarmInfo.AckTime = Now
myAlarmInfo.AlarmType = ihALARM_CONDITION
myAlarmInfo.ConditionName = "SampleCondition"
myAlarmInfo.DataSourceName = "SampleDataSource"
myAlarmInfo.Source = "SampleSource"
myAlarmInfo.StartTime = AlarmStartTime
myAlarmInfo.SubConditionName = "HIHI"
myAlarmInfo.Timestamp = Now
myAlarmInfo.Quality = 3
myAlarmInfo.Add MyServer myAlarmInfo.Clear
' Return to Normal
myAlarmInfo.AlarmType = ihALARM_CONDITION
myAlarmInfo.ConditionName = "SampleCondition"
myAlarmInfo.DataSourceName = "SampleDataSource"
myAlarmInfo.EndTime = Now
myAlarmInfo.Source = "SampleSource"
' Not required, but pointing out the start time of the alarm doesn't hurt
myAlarmInfo.StartTime = AlarmStartTime
myAlarmInfo.Timestamp = Now
myAlarmInfo.Quality = 3
myAlarmInfo.Add MyServer
myAlarmInfo.Clear