General Reference

Metrics and Scorecards Security Groups

The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned. In Essentials, Roles are assigned to Security Users through permission sets.

Important: Assigning a Security User to a Role grants that user the privileges associated with all of the Security Groups that are assigned to that Role. To avoid granting a Security User unintended privileges, before assigning a Security User to a Role, be sure to review all of the privileges associated with the Security Groups assigned to that Role.
Security GroupRoles
MI Metrics Administrator

MI Foundation Admin

MI Metrics User

MI  Foundation Power

MI Foundation User

MI Metrics ViewerMI APM Viewer
Everyone

MI Foundation Admin

MI Foundation Power

MI Foundation User

The baseline family-level privileges that exist for these Security Groups are summarized in the following table.

Family

MI Metrics Administrator

MI Metrics User

MI Metrics Viewer
Entity Families
KPIView, Update, Insert, DeleteView, Update, Insert, DeleteView

KPI Measurement

View, Update, Insert, Delete View, Update, Insert, Delete View
ScorecardView, Update, Insert, Delete View, Update, Insert, Delete View
Relationship Families
Has KPI MeasurementView, Update, Insert, DeleteView, Update, Insert, DeleteView
Has PrivilegesView, Update, Insert, DeleteView, Update, Insert, DeleteView
Has Sub IndicatorsView, Update, Insert, DeleteView, Update, Insert, DeleteView
Is Used By ScorecardView, Update, Insert, DeleteView, Update, Insert, DeleteView

In addition to performing functions associated with the family-level privileges described in this table, members of the MI Metrics Administrator Security Group has full access to all KPIs and Scorecards without needing to be granted additional privileges via Essentials.

Metrics and Scorecards Data Model

The following diagram illustrates how the entity and relationship families that are used in Metrics and Scorecards are related to one another. The shaded boxes represent entity families, and the arrows represent relationship families. You can determine the predecessor and successor in each relationship definition from the direction of the arrow head:
  • The box from which the arrow originates is the predecessor in that relationship definition.
  • The box to which the arrow head points in the successor in that relationship definition.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

In this image, you can see that:

  • KPI records can be related to other KPI records through the Has Sub-Indicators relationship.

Metrics and Scorecard Security Groups

The following baseline Security Groups are provided for the Metrics and Scorecards module:

  • MI Metrics Administrator: Provides users with full access to all Metrics and Scorecards features and functions.
  • MI Metrics User: Provides users with view-only access to Metrics and Scorecards functionality, provided that they have been granted the necessary entity-level permissions.

The baseline privileges for these Security Groups are summarized in the following table.

FamilyMI Metrics AdministratorMI Metrics User
KPI View, Update, Insert, Delete View, Update, Insert, Delete
KPI Measurement View, Update, Insert, Delete View, Update, Insert, Delete
Has KPI Measurement View, Update, Insert, Delete View, Update, Insert, Delete
Scorecard View, Update, Insert, Delete View, Update, Insert, Delete
Has Privileges View, Update, Insert, Delete View, Update, Insert, Delete
Has Sub Indicators View, Update, Insert, Delete View, Update, Insert, Delete
Is Used By Scorecard View, Update, Insert, Delete View, Update, Insert, Delete

In addition to performing functions associated with the family-level privileges described in the previous table, members of the MI Metrics Administrator Security Group:

  • Can manage privileges for all KPIs in the Essentials application.
  • Can manage privileges for all Scorecards in the Essentials application.
  • Have full access to all KPIs and Scorecards without needing to be granted additional privileges via the Essentials application.

Metrics and Scorecards URLs

There is one URL route associated with Metrics and Scorecards: metrics. The following table describes the various paths that build on the route, and the elements that you can specify for each.

Tip: For more information, refer to the URLs section of the documentation.
ElementDescriptionAccepted Value(s)Notes
metrics/home: Opens the Metrics and Scorecards page, displaying the Scorecards and the KPIs.
metrics/register-cube: Opens the Manage Cubes page.
metrics/<WorkspaceName>/<EntityKey>: Opens the existing Scorecard and the KPIs.
<Workspace>Specifies the workspace in which you want to open a Scorecard or a KPI.scorecard-tile-viewThe specified Scorecard will appear in the details workspace.
kpi-viewerThe specified KPI will appear in the details page.
kpi-designerThe specified KPI will appear in the design page.
metric-view-designerThe details of the specified Metric Views will appear in the workspace.
<EntityKey>Specifies the level of the asset hierarchy for which you want to view health information. Any numeric Entity Key that corresponds to an existing Scorecard or a KPI.N/A
0Opens a new design page for a Scorecard or a KPI.

Example URLs

Example URLDestination
metrics/home The Metrics and Scorecard page.
metrics/scorecard-designer/0 The design page for a new Scorecard.
metrics/kpi-designer/0 The design page for a new KPI.
metrics/scorecard-tile-view/64253576972 The Scorecard details page for the specified scorecard.
metrics/kpi-viewer/64253550109 The KPI details page for the specified KPI.