SmartSignal Charts
About SmartSignal Charts
SmartSignal charts are time series charts with data plotted measuring value against time.
Up to 60 SmartSignal charts can exist on a single card.
You can plot up to 4000 data points on a SmartSignal Chart.
SmartSignal charts are plotted based on SmartSignal tags, which fetch data from the SmartSignal data source.
From the View Selector, you can access public or private templates, or a Time Series Analysis view.
If you change the date range in the configuration, the data is fetched for the selected date range from the SmartSignal data source and plotted in an analysis view. The x-axis of the chart aligns with the date range and scales from the start date to the end date specified by the user.
If you update or save a new template, the Context Ribbon appears, where you can change the template name, design the template as public or private, and determine if the template is for an instance or a class.
The default date range for a SmartSignal Alert has a start date seven days before the event date and an end date seven days after the event date. You can also choose specific start and end dates if you prefer, but if the current date is earlier than the default end date (seven days after the event), the end date defaults to the current date.
The default date range for a Time Series Analysis View has a start date of 15 days before the current date.
In the workspace, select to access Permissions. Selecting this option gives you the ability to control Visibility, Privileges, and Ownership of specific charts or groups of charts.

- Display Tags as Tag Alias
- Show Template Information
- Show SmartSignal Marker Visibility
- Enable Point Mode for SmartSignal Cards
- Add Card, Connect Gaps
- Use Chart Limits
- Save as New Template
- Set as Default Template
- Update Template
- Delete Template

- Edit Card Name
- Add Cards
- Delete Card
- Export Data
- Export All Charts on This Card As Images
About SmartSignal Cycle Watch Visualization
You can use the SmartSignal Cycle Watch visualization to view the event frames generated by the SmartSignal analytics that are deployed on an asset. This enables you to compare the events over time and identify the anomalies of the assets.
SmartSignal analytics provides you the ability to detect event frames that indicate the operating mode of an asset. The SmartSignal Cycle Watch visualization enables you to view the analytics tags on the asset. You can use the visualization to view the analytics tags within the scope of the events that have been selected for you to view the variance in the output of the tags across multiple instances of the events.
You can view the data associated with the event frames in the Event Frame Analysis mode. Based on the analytics that have been deployed on the asset, you can select the asset for which you want to view the event frames. You can then select the events on the asset for which you want to view the data.
- Save the Event Frame Analysis templates for later use.
- Associate the Event Frame Analysis templates with alert templates and then use them to triage alerts.
Access a Residual Chart
You can display residual charts for specific plotted charts on a SmartSignal card.
About This Task
When you plot a model or a set of tags, some of the tags may contain residual data.
If the Residual toggle is enabled in , you will be able to see residual charts if the residual data exists on the plotted charts.
The residual chart, if present (based on fetched data or user preference selection), also aligns with the date range specified. If there is no data present, the chart does not scale based on the date range.
The residual charts are viewed through the following interactions:
- In ad hoc view, create a SmartSignal card and plot the SmartSignal tags. The residual charts are plotted if residual data is available and you have not disabled the residual charts.
- When navigating from alert to analysis for SmartSignal alerts, the residual charts are plotted if residual data is available and you have not disabled the residual charts.
Procedure
Display a Calculated Tag Formula
You can display the formulas associated calculated tags on a SmartSignal Chart.
About This Task
Some SmartSignal charts have an associated formula that is used to gather the results displayed in the chart. The tags are calculated using the embedded formulas that can be accessed via the chart.
The formulas can be monitored by selecting the calculator icon next to the chart for the formula you want to view.
Procedure
Delete a SmartSignal Chart
You can delete a SmartSignal chart in the Analysis view.
About This Task
If you delete a SmartSignal chart, the chart is deleted and all the tags associated to the deleted chart are removed from the plotted tags list.
Procedure
Export a SmartSignal Chart as a .PNG Image
About This Task
Procedure
- In the Applications menu, navigate to the HEALTH section, and then select Analysis.
- Use the Context Browser to select an SmartSignal asset context.
- In the chart type list, select a chart.
- Plot the tags.
- Select Gear, and then select Export As Image.
- The .PNG image is saved to the local computer.
- Select the image, and then select Open.
- Save the image.
Export a SmartSignal Chart in .CSV Format
About This Task
Procedure
- In the Applications menu, navigate to the HEALTH section, and then select Analysis.
- Use the Context Browser to select an SmartSignal asset context.
- In the chart type list, select a chart.
- Plot the tags.
- Select List, and then select Export Data.
- The .CSV file is saved to the local computer.
- Select the file, and then select Open.
- Save the Excel file.
Display Diagnostic Markers and Alert Information on SmartSignal Charts
You can display diagnostics markers on the SmartSignal charts if the analytics on the tags have detected any anomalies.
Procedure
Access Parent-Level Asset for an Asset Using an Alert
This topic describes how to access the parent-level asset for an asset using an analysis template linked to the alert that is associated with the asset.
Procedure
Access Parent-Level Asset for an Asset Using a Case
This topic describes how to access the parent-level asset for an asset using the analysis templates linked to the case that is associated with the asset.
Procedure
Add or Update a Cross-Hair on a SmartSignal Chart
About This Task
Procedure
Add SmartSignal Tags to a SmartSignal Card
You can add a SmartSignal tag or a group of SmartSignal tags to a SmartSignal card.
Procedure
Configure the SmartSignal Series Settings at the Card Level
This topic describes how to set the SmartSignal chart series configuration at the card level.