Publish Log and Version
After you publish the MQTT plugin changes, you can directly view the published log
reports by clicking the icon.

Publish Log
To view the publish log reports:
- Click the MQTT plugin overflow
icon.
- Select Publish Log.
The Publish Report dialog appears.
Table 1. MQTT Publish Log Report Field Description Operation Indicates whether the operation is added, modified, or deleted. Broker Name Name of the Broker. Subscription Name Name of the Subscription. Timestamp (YY-MM-DD HH:mm:ss) Record of the event in the format YY-MM-DD HH:mm:ss. - Select the OPC UA tab to view the OPC UA log reports.
Table 2. OPC UA Publish Log Report Field Description Key The key refers to the field names in the OPC UA Settings page. Value The value entered in the fields of the OPC UA Settings page. Status The status of the published log information. Timestamp (YY-MM-DD HH:mm:ss) Record of the event in the format YY-MM-DD HH:mm:ss. Note:- You can click the
icon to filter the data as required.
- You can click the Download Log button to download the log information.
- You can click the
Important: Only the last published log information will be
displayed in the Publish Report window.
Version
You can click the MQTT plugin overflow
icon, and then select
Version.


The Version Details dialog appears.
The MQTT Client application version details are displayed.