Install Collectors Using the Installer
About this task
- Executable files: These files are required to add a collector instance.
- Instances of the following collectors:
- The iFIX collector
- The iFIX Alarms & Events collector
- The OPC Classic Data Access collector for CIMPLICITY
- The OPC Classic Alarms and Events collector for CIMPLICITY
- The Remote Collector Management agent: Provides the ability to manage collectors remotely.
You can also install them at a command prompt.
Procedure
- Run the InstallLauncher.exe file.
-
Select Install Collectors.
The welcome page appears.
-
Select Next.
The license agreement appears.
-
Select the Accept check box, and then select
Next.
The default installation drive appears.
-
If needed, modify the installation drive, and then select
Next.
The data directory page appears.
-
If needed, change the folder for storing the collector log files, and then select
Next.
The destination Historian server page appears.
-
Provide the credentials of the Windows user account of the destination Historian server
to which you want Remote Management Agent to
connect.
These details are required for Remote Collector Manager to connect to Historian to manage the collectors remotely. If are installing collectors on same machine as the Historian server, and if strict collector authentication is disabled, you need not provide these details; by default, the machine name of the local Historian server is considered. If, however, they are installed on different machines, or if strict collector authentication is enabled, you must provide the credentials of the Historian server user.
-
Select Next.
A message appears, stating that you are ready to install collectors.
-
Select Install.
The installation begins.
- When you are prompted to reboot your system, select Yes.
Results
- HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\ GE Digital\iHistorian\Services\<collector type>
- HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\iHistorian\Services\<collector type>
- The iFIX collector
- The iFIX Alarms & Events collector
- The OPC Classic Data Access collector for CIMPLICITY
- The OPC Classic Alarms and Events collector for CIMPLICITY