Delete a Collector Instance
About this task
This topic describes how to delete a collector instance using Configuration Hub. You can also delete a collector instance using the
RemoteCollectorConfigurator utility, which does not require you to
install Web-based Clients.
Note: When you delete an offline collector instance, the corresponding
configuration file is not deleted. However, if another collector instance of the
same interface name is created, the existing configuration file is replaced by a
template configuration file.
Procedure
- Access Configuration Hub.
-
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Collectors.
A list of collectors appears.Tip: You can filter the collectors by the system name.
-
Right-click the collector instance that you want to delete (or select
), and then select Delete.
A message appears, asking you to confirm that you want to delete the collector instance. - If you want to delete the tags as well, select the Delete associated tags check box.
-
Select Delete.
The collector instance is deleted.