Policy Browse
OPC UA servers are configured with specific security mode and policy. The Details panel of a server connection provides a toolbar button to browse policies .
On execution of this function, the configured Security mode and Policies from the server are browsed and populated into the respective fields in the Details panel.
Select a Security Model and Security Policy to apply to this connection: Basic128Rsa15, Basic256, Basic256Sha256, Aes128_Sha256_RsaOaep, or Aes256_Sha256_RsaPss.
Note: If you are not sure what to select for Security Mode and Security Policy or simply want to test a connection, select None. Be sure that you go back and change this setting later, however, to ensure you have adequate security enabled for your connections.
Note: For the connection to work for any other security policy other than None, you will have to ensure the certificates are properly trusted between the iFIX client and the OPC UA server you are communicating to. See the iFIX help for use of the OPC UA tool in iFIX.