When you stop a collector, the collector stops collecting
data, and it is disconnected from the destination. If, however, you want the collector
to remain connected to the destination, you can instead pause data collection.
A list of collectors linked to the system appears.
Select the row containing the collector that you want to stop.
Select Actions, and then Stop.
The Stop: <collector name> window appears. The COLLECTOR MACHINE and CURRENT RUNNING MODE fields are populated and disabled.
If the collector is running in a Windows service mode, select
Stop. If the collector is running in a command-line
mode, enter values in the Username and
Password fields, and then select
Stop.
The collector is stopped, and the data collection is paused. The status
of the collector in the Collectors section changes to
Stopped.