Log Files

Install Log Files

When installed with iFIX, the log for the Configuration Hub portion of the install is named iFIX 6.5_ConfigHubMSI.log. This log appears in your Windows folder and can be used to troubleshoot any issues that occur during install.

Configuration Hub Log Files

By default, the logs for Configuration Hub are saved to the following location: C:\Program Files (x86)\GE\ConfigurationHub\Logs, by default.

Historian Log Files

For Historian, the logs are stored in the following folder, by default: C:\Proficy Historian Data.

iFIX Log Files

For iFIX, the associated logs are in C:\Program Files (x86)\GE]iFIX\LOCAL\Logs folder, by default. The names of these files are:

Log Name Description

ifix_auth_service.log

iFIX authentication service log file.

ifix_config_service.log

iFIX OPCUA Config Service log file.

ifix_config_service_cert.log

Self-Signed Certificate creation utility log file. This log file is automatically overwritten on each iFIX startup.

ifix_confighub_facade_service.log

iFIX ConfigHub Facade service log file.

ifix_model_editor_service.log

Model editor service log file.

ifix_model_service.log

iFIX model service which is used for publishing model information to iFIX.

ifix_tag_service.log

iFIX tag service log file.
IGS Log File

For IGS, the log file named igs-browse-config.log is located in the C:\Program Files (x86)\GE\iFIX\LOCAL folder, by default.