Access Collector Statistics
About this task
Procedure
- Open an Excel worksheet.
-
Select
.The Historian Collector List window appears.
- Select a server from the drop-down list. If you do not specify a server, the default server is considered.
-
Enter values as described in the following table.
Field Description Collector Name Enter a collector instance name. Do not use wildcards in this field. Tip: To return details for more than one item, specify a substring in the Collector Name field that exists in each collector you want listed. For example, if you have collectors named fromHero5_Collector0001
toHero5_Collector010
, enterHero5_Collector
to return the details for all those collectors.Output Display Select one or more parameters for the output display. Output Range Select a range of cells in a single row or column to determine where the returned data is placed. - Select either Columns or Rows for the output display.Note: When selecting multiple tags, the orientation of the return data is based on the orientation of the selected tags and the Row/Col selection is ignored.
-
Select OK.
The statistics of the selected collector instances appear.